What library can be customized?
The
RAMSCustom.dll
is the compiled version of the insertion point DLL
for the Material Server and is where custom rules are defined.
RAMSCustom.dll
is required for operation of the Material Server,
resides in the Batch\bin
directory, and is registered during the
installation of Material Manager.A C# project is provided on the
FactoryTalk Batch
Material Manager
installation CD, in a folder called Custom
,
so you can create a custom version of the RAMSCustom.dll
.Provide Feedback