Using manual phase control
Use
FactoryTalk Batch View
to command a material-based phase using manual phase
control in Equipment
.
WARNING:
If communication with the Material Server fails while in Equipment, and the material policy option is configured for Switch to Manual, all containers associated with the phase display. The list is not filtered by the selected material. Use extreme caution when operating without the Material Server. Failure to select the correct container or phase pair could result in a hazardous situation, depending on the material.
To command a material-based phase using manual control
- SelectEquipment.
- Select the material-enabled phase to acquire and selectAcquire
. - If prompted, confirm the command.TIP:The manual phase control session requests ownership of the phase (and OPERATOR will appear in the phase’s Needed By list). The phase must be released by the control recipe, and then the operator acquires the phase.
- SelectStart
. - If prompted, confirm the command.
- If the phase is configured as both a material distribution and addition, from theFeed Typelist, select the type for the phase.TIP:If the phase is not configured as both a material distribution and addition, the configuredFeed Typefor the material phase cannot change.
- Select a material to use from theMateriallist, and selectContinue.
- Enter a unique batch ID.
- (optional) If a phase has a control strategy, select the strategy from theControl Strategybox.
- Select a container, and selectOK. The batch state displaysDOWNLOADING.TIP:If the phase has automatic uploads and downloads,Promptsshows the prompt(s) to acknowledge.
- If prompts generate for the phase, selectPrompts.TIP:If prompts are present, anx Promptslink displays in the left sidebar navigation. Selecting thePromptslink goes to thePromptslist, displaying only the prompts for that phase.
- InPrompts, select the prompt, enter the appropriate value, and selectAcknowledge
. - Once the phase completes, select the phase, and then selectReset
. - With the phase still selected, selectRelease
.
Provide Feedback