OnGenerateCustomLotName

Problem to be solved
Composite containers can hold only one sublot at a time. If the composite container holds a sublot of LOT_A and a sublot of LOT_B is added to the container, the sublots are assumed to be mixed together and become a single sublot. What lot should the mixture belong to?
This insertion point allows you to define the lot to which a sublot formed by combining sublots of different lots will belong. This can be an existing lot or a new lot.
Specifics about this routine
This insertion point is only called when sublots of different lots are being combined by a composite container. These are the parameters for this function:
Function parameters
Param Name
Data Type
Direction
Description
DistributionAmount
Double
In
Amount of the distribution
MaterialName
String
In
Name of Material
DistributionLotName
String
In
Lot name given to the distribution
AreaName
String
In
Area Name
StepName
String
In
Step Name
ProcessCell*
String
In
Process Cell
UnitName*
String
In
Unit Name
BatchID
String
In
Batch ID
EqModule
String
In
Equipment Module
RecipePath
String
In
Recipe Path
ContainerName
String
In
Container name of the distribution
ExistingLotName
String
In
Lot name that exists in the Container
CustomLotName
String
Out
Returned value from the event
This value represents what the custom Lot name will be based on in the insertion code.
Related insertion points
Other insertion points that could work with this function include:
  • OnGenerateCustomLabelName
  • AfterSublotDelete
  • AfterSublotInsert
  • AfterCombinedLotInsert
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal