OnGenerateCustomLabelName

Problem to be Solved
Composite containers can hold only one sublot at a time. If the composite container holds a sublot with the label "LABEL_1" and a sublot with the label "LABEL_2" is added to the container, the sublots are assumed to be mixed together and become a single sublot. What label should the mixture be assigned?
This insertion point allows the customer to define the label to be assigned to a sublot when two sublots with different labels are combined by a composite container.
Specifics About this Routine
This insertion point is only called when sublots with different labels are being combined by a composite container. These are the parameters to this function:
Function parameters
Param Name
Data Type
Direction
Description
DistributionAmount
Double
In
Amount of the distribution
MaterialName
String
In
Material Name
DistributionLabelName
String
In
Label name given to the distribution sublot
AreaName
String
In
Area Name
StepName
String
In
Step Name
ProcessCell*
String
In
Process Cell Name
UnitName*
String
In
Unit Name
BatchID
String
In
Batch ID
EqModule
String
In
Equipment Module
RecipePath
String
In
Recipe Path Name
ContainerName
String
In
Container name of the distribution
ExistingLabelName
String
In
Label name that exists in the Container
CustomLabelName
String
Out
Returned value from the event
This value represents what the custom Label name will be based on the business rules in the insertion code.
Related insertion points
Other insertion points that could work with this function include:
  • OnGenerateCustomLotName
  • AfterSublotDelete
  • AfterSublotInsert
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal