Manually assign prompted material phase binding to a material phase step
Prompted material phase binding is the process of binding a material phase after a prompt
is generated. Only those requirements defined with the
Prompted
Binding
method generate a prompt. When prompted material phase binding is set up, the execution of the batch pauses when the transition above the unbound step becomes true.
To manually assign prompted material phase binding to a material phase step
- OpenFactoryTalk Batch Viewand selectBatches.
- Select a batch.
- In theBatch Detaildisplay, select a material step.
- SelectBind
. - InBinding a Material Phase Step, selectPrompt.
- SelectOK.
Provide Feedback