UpdateTestSpecification

Updates a QA test specification record in the material database.
Syntax
Material
.
UpdateTestSpecification
(
TestSpecification
As TestSpecification)
The
UpdateTestSpecification
method syntax has these parts:
UpdateTestSpecification parts
Part
Description
Material
Instance of the Material interface to which the method is directed.
TestSpecification
An instance of a TestSpecification object.
Remarks
This interface will allow for the modification of a QA test specification after it is added to the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal