UpdateMaterialClassProperty
Updates a MaterialClassProperty record in the material database.
Syntax
MaterialClass.UpdateMaterialClassProperty
(MaterialClassProperty
As MaterialClassProperty), PropagateChanges
As Boolean,
[ActivityDescription
As String])The
UpdateMaterialClassProperty
method syntax has these parts:Part | Description |
|---|---|
MaterialClass | Instance of the MaterialClass public interface to which the method is directed. |
MaterialClassProperty | An instance of a MaterialClassProperty object. |
ActivityDescription | Adds descriptive text to the activity journal for this operation.
( Optional ) |
Provide Feedback