UpdateMaterial
Updates a Material record in the material database.
Syntax
MaterialSvr.UpdateMaterial
(Material
As Material,
[ActivityDescription
As String])The
UpdateMaterial
method syntax has these parts:Part | Description |
|---|---|
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
Material | An instance of a Material object. |
ActivityDescription | Adds descriptive text to the activity journal for this operation.
( Optional ) |
Provide Feedback