UpdateLotState

Updates a LotState record in the material database.
Syntax
MaterialSvr.UpdateLotState
(
LotState
As LotState)
The
UpdateLotState
method syntax has these parts:
UpdateLotState parts
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
LotState
An instance of a LotState object.
Remarks
The ‘Ready To Use’ LotState is a system-defined state and cannot be updated via this method or any other means.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal