UpdateContainerProperty

Updates a ContainerProperty record in the material database.
Syntax
Container.UpdateContainerProperty
(
ContainerProperty
As ContainerProperty, [
ActivityDescription
As String])
The
UpdateContainerProperty
method syntax has these parts:
UpdateContainerProperty parts
Part
Description
Container
Instance of the Container object to which the method is directed.
ContainerProperty
An instance of a ContainerProperty object.
ActivityDescription
Adds descriptive text to the activity journal for this operation. (
Optional
)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal