UpdateContainer

Updates a Container record in the material database.
Syntax
MaterialSvr.UpdateContainer
(
Container
As Container, [
ActivityDescription
As String])
The
UpdateContainer
method syntax has these parts:
UpdateContainer parts
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
Container
An instance of a Container object.
ActivityDescription
Adds descriptive text to the activity journal for this operation. (
Optional
)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal