InsertSubLot

Inserts a SubLot record into the material database.
Syntax
Container.InsertSubLot
(
SubLot
As SubLot)
The
InsertSubLot
method syntax has these parts:
InsertSubLot parts
Part
Description
Container
Instance of the Container object to which the method is directed.
SubLot
An instance of a SubLot object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal