InsertMaterialType

Inserts a Material Type record into the material database.
Syntax
MaterialSvr
.
InsertMaterialType
(
MaterialType
As MaterialType)
The
InsertMaterialType
method syntax has these parts:
InsertMaterialType parts
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
MaterialType
An instance of a MaterialType object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal