InsertMaterialProperty

Inserts a MaterialProperty record into the material database.
Syntax
Material
.
InsertMaterialProperty
(
MaterialProperty
As MaterialProperty)
The
InsertMaterialProperty
method syntax has these parts:
InsertMaterialProperty parts
Part
Description
Material
Instance of the Material Interface to which the method is directed.
MaterialProperty
An instance of a MaterialProperty object.
Remarks
When inserting a Material Property record, the Material Server will add an accompanying Lot Property for every Lot that is derived from the specified Material.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal