InsertErrorCorrection
Inserts a QA error correction record associated with a test specification in the material database.
Syntax
MaterialSvr
.InsertErrorCorrection
(ErrorCorrection
As ErrorCorrection)The
InsertErrorCorrection
method syntax has these parts:Part | Description |
|---|---|
MaterialSvr | Instance of the MaterialSvr interface to which the method is directed. |
ErrorCorrection | An instance of a ErrorCorrection object. |
Remarks
This interface will allow for the creation of QA error corrections in the material database.
Provide Feedback