InsertContainerProperty

Inserts a ContainerProperty record into the material database.
Syntax
Container
.
InsertContainerProperty
(
ContainerProperty
As ContainerProperty)
The
InsertContainerProperty
method syntax has these parts:
InsertContainerProperty parts
Part
Description
Container
Instance of the Container object to which the method is directed.
ContainerProperty
An instance of a ContainerProperty object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal