InsertContainerMaterial

Inserts a ContainerMaterial record into the material database.
Syntax
Container
.
InsertContainerMaterial
(
ContainerMaterial
As ContainerMaterial)
The
InsertContainerMaterial
method syntax has these parts:
InsertContainerMaterial parts
Part
Description
Container
Instance of the Container object to which the method is directed.
ContainerMaterial
An instance of a ContainerMaterial object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal