GetStorageLocation
Returns a StorageLocation object populated with the specified StorageLocation data from the material database, based on the Storage Location Name.
Syntax
Set
object
=
MaterialSvr
.GetStorageLocation
(ByVal sName
As String, UseCollection
As Boolean)The
GetStorageLocation
method syntax has these parts:Part | Description |
|---|---|
object | Reference to a valid StorageLocation object. |
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
sName | Represents the ID of the StorageLocation record from the material database. |
UseCollection | True: Attempts to locate the specified StorageLocation in
a pre-populated collection. If no collection is present, one is created and the
record is read from the collection.False: Reads the record directly from the database. |
Provide Feedback