GetMaterialClassByID

Returns a MaterialClass object with its properties populated with corresponding data from the material database, based on the MaterialClassID.
Syntax
Set
object
=
MaterialSvr
.
GetMaterialClassByID
(ByVal
MaterialClassID
As Long)
The
GetMaterialClassByID
method syntax has these parts:
GetMaterialClassByID parts
Part
Description
object
Reference to a valid MaterialClass object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
MaterialClassID
Represents the ID of the MaterialClass.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal