GetMaterialClass

Returns a MaterialClass object that is populated with the specified MaterialClass data from the material database, based on the MaterialClass Name.
Syntax
Set
object
=
MaterialSvr
.
GetMaterialClass
(ByVal
MaterialClassName
As String,
UseCollection
As Boolean)
The
GetMaterialClass
method syntax has these parts:
GetMaterialClass parts
Part
Description
object
Reference to a valid MaterialClass object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
MaterialClassName
Represents the name of the MaterialClass.
UseCollection
True:
Attempts to locate the specified MaterialClass in a pre-populated collection. If no collection is present, one is created and the record is read from the collection.
False:
reads the record directly from the database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal