GetMaterialByID

Returns a Material object with its properties populated with corresponding data from the material database, based on the MaterialID.
Syntax
Set
object
=
MaterialSvr
.
GetMaterialByID
(ByVal
IMaterialID
As Long)
The
GetMaterialByID
method syntax has these parts:
GetMaterialByID parts
Part
Description
object
Reference to a valid Material object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
IMaterialID
Represents the ID of the Material.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal