GetLotList
Returns a list of Lots. This is a string representing the material name that is used by the ContainerFilter to filter on in a multi-dimensioned array.
Syntax
vResult
= MaterialSvr
.GetLotList
(ByVal
LotFilter As
LotFilterEnum, ByVal FilterValue
As String)The
GetLotList
method syntax has these parts:Part | Description |
|---|---|
vResult | The data returned by the Material Server. |
MaterialSvr | Instance of the MaterialServer Batch Interface to which the method is directed. |
LotFilter | An enumeration representing a set of pre-defined filters: 0 = GetAllLots 1 = ByMaterialName |
FilterValue |
Where
vResult
is:Part | Description |
|---|---|
vResult | Is a two-dimensional array containing <Empty Array> | <LotData> |
LotData | Array Element [0] = PKid Array Element [1] = Lot Name Array Element [2] = Description Array Element [3] = ControllerID |
Remarks
In order to test for an empty array, you must test the upper and lower bounds of the
vContainerList
array. If both bounds are zero, then the array is empty and
can be treated as such.Provide Feedback