GetContainerPriorityListByContainer

Returns a collection of 1 to N ContainerPriority objects.
Syntax
Set
object
=
MaterialSvr
.
GetContainerPriorityListByContainer
(
ContainerName
As String)
The
GetContainerPriorityListByContainer
method syntax has these parts:
GetContainerPriorityListByContainer parts
Part
Description
object
Reference to a valid ContainerPriorities collection object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
ContainerName
String representing the name of the Container you want to produce the list from.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal