GetContainerByID
Returns a Container object with its properties populated with corresponding data from the material database, based on the ContainerID.
Syntax
Set
object
=
MaterialSvr
.GetContainerByID
(ByVal
ContainerID
As Long)The
GetContainerByID
method syntax has these parts:Part | Description |
|---|---|
object | Reference to a valid Container object. |
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
ContainerID | ID of the Container being requested. |
Remarks
Although this method loads the Container data of the Container object, this object contains a collection of ContainerProperties and ContainerMaterials. These collection objects are not populated until you explicitly call those properties on the Container object. The purpose for this is that pre-loading these collection objects is a performance hit that need not be taken unless those particular elements are required.
Provide Feedback