DeleteTestSpecification
Deletes a QA test specification record from the material database.
Syntax
Material
.DeleteTestSpecification
(TestSpecification
As TestSpecification, ForceDelete
as Boolean)The
DeleteTestSpecification
method syntax has these parts:Part | Description |
|---|---|
Material | Instance of the Material interface to which the method is directed. |
TestSpecification | An instance of a QATestSpec object. |
ForceDelete | TRUE | FALSE TRUE deletes the test specification and all details.FALSE deletes the test specification if there is no detail
information. FALSE is the default for the argument, so the user must explicitly
set to TRUE to cause a force delete to occur. |
Remarks
This interface will not only delete the QA test specification — it will also delete all QA test specification details that are a part of the test specification.
The
ForceDelete
argument allows the user to delete a test specification and
all associated test result data by setting the value to TRUE. If the value is set to FALSE
and the test specification has associated test results, the test specification cannot be
deleted.Provide Feedback