DeleteTestResult

Deletes a QA test result record associated with a test specification in the material database.
Syntax
TestSpecification
.
DeleteTestResult
(
TestResult
As TestResult)
The
DeleteTestResult
method syntax has these parts:
DeleteTestResult parts
Part
Description
TestSpecification
Instance of the QATestSpec interface to which the method is directed.
TestResult
An instance of a TestResult object.
Remarks
This interface allows for the deletion of QA test results from the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal