DeleteStorageLocation

Deletes a StorageLocation record from the material database.
Syntax
MaterialSvr
.
DeleteStorageLocation
(
StorageLocation
As StorageLocation, [
ActivityDescription
As String])
The
DeleteStorageLocation
method syntax has these parts:
DeleteStorageLocation parts
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
StorageLocation
An instance of a StorageLocation object.
ActivityDescription
Adds descriptive text to the activity journal for this operation. (
Optional
)
Remarks
A StorageLocation can only be deleted if there are no Containers using it. There is no provision in this method to override this functionality, nor is there a way to unassociate the Containers that are using the StorageLocation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal