DeleteLimit

Deletes a QA test specification limit record associated with a base test specification in the material database.
Syntax
TestSpecification
.
DeleteLimit
(
TestSpecificationLimit
As TestSpecificationLimit)
The
DeleteLimit
method syntax has these parts:
DeleteLimit parts
Part
Description
TestSpecification
Instance of the QATestSpec interface to which the method is directed.
TestSpecificationLimit
An instance of a TestSpecificationLimit object.
Remarks
This interface allows for the deletion of a QA test specification limit record from the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal