DeleteErrorCorrection

Deletes a QA error correction record associated with a test specification in the material database.
Syntax
MaterialSvr
.
DeleteErrorCorrection
(
ErrorCorrection
As ErrorCorrection)
The
DeleteErrorCorrection
method syntax has these parts:
DeleteErrorCorrection parts
Part
Description
MaterialSvr
Instance of the MaterialSvr interface to which the method is directed.
ErrorCorrection
An instance of an ErrorCorrection object.
Remarks
This interface allows for the deletion of QA error corrections from the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal