CreateTestResult

Inserts a QA test result record associated with a test specification in the material database.
Syntax
TestSpecification
.
CreateTestResult
(
TestResult
As TestResult,
Lot
As Lot)
The
CreateTestResult
method syntax has these parts:
CreateTestResult parts
Part
Description
TestSpecification
Instance of the TestSpecification interface to which the method is directed.
TestResult
An instance of a TestResult object.
Lot
An instance of the Lot object that the test specification is being executed against.
Remarks
This interface allows for the creation of QA test results in the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal