Start the FactoryTalk Batch and Material Manager Servers
The
FactoryTalk Batch
and Material Manager
Servers may start automatically when the computer starts. By default, the FactoryTalk Batch
Server starts in production mode. If FactoryTalk Batch
has not been activated, the tutorial can run in demo mode. While in demo mode, the FactoryTalk Batch
Server runs for a two-hour period and then stops.
TIP:
The
FactoryTalk Batch
Server does not start in production mode without
activation. The Material Manager
Server starts automatically when the FactoryTalk Batch
Server starts. See Activating
for more information.Material Manager
To start or restart the
FactoryTalk Batch
Server:- Select .IMPORTANT:If you are logged in with an account that does not have administrator privileges, right-clickBatch Service Managerand select to run under elevated privileges.
- In theFactoryTalk Batch Service Manager, select theFactoryTalk BatchServer if it is not listed in theServicebox.
- If theFactoryTalk BatchServer is running, selectStop.
- If the name of the computer where theFactoryTalk BatchServer is installed does not display in theComputerbox, select theSelect Computerbutton.
- In theSelect Computerdialog underEnter the object name to select, type the name of the computer where the Batch Server is installed (or selectAdvancedto search for a computer). SelectOK.TIP:TheFactoryTalk BatchService Manager must communicate with the Windows Service Manager of the selected computer to determine what services are available. There may be a noticeable delay when establishing communications. If the Service Manager cannot communicate with the Windows Service Manager of the selected computer, a message displays.
- From theServicelist, selectFactoryTalk Batch Server.TIP:IfNo Batch Servicesdisplays in the list, theFactoryTalk BatchServer is not installed on the selected computer. See the for installation instructions.
- To start theFactoryTalk BatchServer in Demo mode, selectAllow Demo Mode.
- Select the method to use for restarting the server.Server restart methodsMethodDescriptionCold RestartTheFactoryTalk BatchServer starts in a new instance without restoring data from its previous run. Batches are not added back to the batch list, and operator arbitration states are not recovered. For all batches that were not restored, batch completion events are recorded in theFactoryTalk BatchEvent Journals. After a Cold Restart, you will not be able to resume execution of batches from the previous instance. If Security Authority is enabled, SAIs in a secured area model and any secured recipes must match the current Network FactoryTalk Directory SAI.Warm RestartRestarts theFactoryTalk BatchServer and attempts to restore the set of batches that were on the batch list when the server previously stopped. Batch complete events are added to theFactoryTalk BatchEvent Journals for all batches that were not restored to the batch list. After a Warm Restart, any batches that are not restored cannot be recovered or resumed in the future. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.Warm All RestartTheFactoryTalk Batchserver attempts to restart but will not restart if it is unable to restore all the batches to the batch list. If a Warm All Restart attempt fails, the ability to restore batches in the future is not affected. After the issues are resolved, another attempt to restore the batches to the batch list can be made using Warm Restart, Warm All Restart, or Hot Restart. This is the default setting for automatic restarts. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.Hot RestartFollows all the startup rules of Warm All Restart. In addition, theFactoryTalk BatchServer attempts to restore batches to their last known state, including transition states and recipe modes, without any operator interaction.
- Select theStart/Continuebutton. The Service State area changes from STOPPED to START PENDING. After a few moments, RUNNING displays and the light changes to green. The Material Server starts automatically with theFactoryTalk BatchServer.TheFactoryTalk BatchPhase Simulator starts automatically. Minimize the window.
- SelectCloseto close theFactoryTalk BatchService Manager.TIP:If conversation becomes LOST while running in Demo mode, make sure that the Simulator is running and try starting the server(s) again. SeeStarting thefor more information.FactoryTalk BatchPhase Simulator
Provide Feedback