Summary
In this chapter, you:
- Created a material-based operation
- Created recipe formula parameters
- Assigned formula values
- Created a unit procedure
- Linked phase groups
This chapter provided a brief overview of the capabilities of the Recipe Editor when used
with Material Manager. [See the for more
information on creating material-based recipes, unit binding, and linking phase groups.]
FactoryTalk Batch Recipe
Editor User Manual
, publication BATCH-UM006
Provide Feedback