Enabling dynamic unit allocation
To support the flexibility of the two units within NORTH_PARLOR process cell, you want to enable dynamic unit allocation, which will provide more binding options.
- From theViewmenu, selectOptions. TheOptionsdialog opens.
- If necessary, enableSupport Dynamic Unit Allocation, and then clickApply.
- Save the unit procedure. If prompted, enter auditing comments, if desired, and clickOK.
Provide Feedback