Creating recipe formula parameters

Because you want to defer the amounts of the materials at this level in the recipe, you need to add formula parameters. You will enter default amounts at the procedure level and the operator will have an opportunity to change the amount when the batch is added to the batch list.
  1. From the
    Recipe
    menu, select
    Recipe Parameters/Reports
    . The
    Procedure Properties
    dialog opens.
  2. Click the
    Add Parameter
    button.
  3. In the
    Name
    box, type
    COCOA_AMT
    .
  4. In the
    Max
    box, type
    500
    .
  5. In the
    Enum/EU
    box, type
    KG
    .
  6. Select
    Scalable
    .
  7. Click the
    New
    button, and then add
    HAZELNUT_AMT
    with the same values.
    FTBMM_GRG_recipe_formula_parameter_list
  8. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal