Security requirements

The FactoryTalk Batch components have been developed to take advantage of Windows’ built-in security features. Material Manager supports two types of security schemes – Domain or Workgroup. Each of these schemes are also supported in the security defined within the Material Server’s database security scheme. There are a number of procedures involved in the implementation of Material Manager security, some of which must be performed prior to the installation and implementation of Material Manager. Review your facility’s security requirements and determine the most appropriate security scheme for your implementation. You should include a detailed list of security requirements within your implementation plan. [Refer to the for complete information on supported security schemes.]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal