Configuring the material display
You can display the materials in list form (default) by type or by class. If you choose to display by type or class, you can select to display only certain types or classes of materials.
- From theUser Preferencesdialog select theMaterialstab.
- In theMaterials Display Formatarea, select the desired display format:
- List(default)Displays the materials in alphabetical list form (as shown)

- By TypeDisplays the materials by their type (for example; Finished, Intermediate, or Raw) or you can select all three to display the materials in a hierarchy view by type (as shown).

- By ClassDisplays the materials by their class designation (for example; Colorings, Flavorings, etc.) or you can select all classes to display the materials in a hierarchy view by class (as shown).

- ClickApply. The Material list is refreshed, with the display format applied.
Provide Feedback