Changing list view properties

The
List View Properties
area contains the following options to change the appearance and behavior of items seen in a list view.
  • "Hot" list selection
    – If selected, an item is automatically highlighted and selected when the cursor remains over the item for a certain period of time.
  • List information tips
    – If selected, single-line tips appear when you move the cursor over a button or field. See Editing information tips for more information.)
  • Flat scroll bars
    – If selected, scroll bars appear 2‑dimensional. If disabled, scroll bars have a 3‑dimensional appearance (Windows default). The following figure illustrates both the default (on the left) and flat (on the right) scroll bars:
    FTB_scrollbars
  • Header drag and drop
    – If selected, users can click and drag a header from one location to another in order to rearrange the columns.
  • Header "hot" tracking
    – If selected, an item is automatically highlighted but not selected when the cursor moves over a header item. You must still click the item at least once to activate it.
  • Subitem images
    – Not currently enabled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal