Changing margins
- To change the margins, fonts, and colors of a printed report, click the desiredReportbutton (List, Formatted, or Graphical). TheReport Page Configurationdialog opens.

- Change the margin widths of the printed report if desired. Type the desired amounts in each box for theLeft,Right,Top, andBottommargins. A visual representation of each margin change displays in theReportpage preview area. Note that this is not to scale.
- If you want to use inches instead of metric measurements, disableMetric Measurements.
- ClickOKto close theReport Page Configurationdialog.
- ClickApply.
Provide Feedback