Printing reports
- In the Editor’s Hierarchy pane, select the list or item(s) that you want to print.
- From theFilemenu, clickPrint. You could also click thePrintbutton or pressCtrl+Pto display thePrintdialog.
- Ensure that the correct printer is selected, and clickOK.TIP:To configure heading and footer fonts, and add a custom footer to your reports, see Setting report preferences for instructions.
Printing a Range of Reports
Occasionally, you may want to print just certain pages of the report. You can do so by entering the starting and ending page numbers of the section you want printed.
- In the Editor’s Hierarchy pane, select the list or item(s) that you want to print.
- ClickPrint.
- In thePage Rangearea, clickPages. Type the page numbers to print in theFromandToboxes.
- Ensure that the correct printer is selected and clickOK.
Provide Feedback