Deleting storage locations
- To delete a location, right-click on a location and selectDelete.
- IfConfirm deletionis enabled on theUser Preferencesdialog, a confirmation message about the selected location opens. To delete the location, clickYes.IfConfirm deletionis disabled on theUser Preferencesdialog, the storage location is deleted without a confirmation message. (See Configuring the Material Editor for more information on defining the user preferences.)TIP:You cannot delete a material storage location that has material storage containers assigned to it. You must either reassign or delete the containers, and then you can delete the storage location.
Provide Feedback