Editing container properties

  1. From the
    Edit Material Storage Container
    dialog, select a record number to edit and click the
    Edit Property
    button.
    FTBMM_ED_Storage Container_Edit Properties
  2. Modify the container property as needed, and then click
    OK
    .
    IMPORTANT:
    If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
  3. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal