Deleting materials

  1. In either the
    Hierarchy
    pane or
    Detail
    pane, right-click the material to delete, and then click the
    Delete
    button.
  2. If the
    Confirm deletion
    user preference is enabled, you are asked to verify the deletion. To delete the material, click
    Yes
    ; to cancel the deletion, click
    No
    .
    If the
    Confirm deletion
    user preference is disabled, the selection is deleted without a confirmation message. (See Configuring the Material Editor for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal