Editing material properties
- If theEdit Materialdialog is open, select thePropertiestab.If not, right-click on a material in theHierarchyorDetailpane, and selectProperties. TheEdit Materialdialog opens. Select thePropertiestab. The currently defined material properties display in a table format. You can also use a form to make changes.
For inherited material class properties, you can change only the minimum, maximum, and default values. - Modify the material property as desired.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.TIP:Changing a duplicate property that is assigned to other materials does not affect the other properties.
Provide Feedback