Deleting material properties

  1. From the
    Edit Materials
    dialog, select a record row to delete, and then click the
    Delete Property
    button.
  2. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog box.
    TIP:
    Deleting a duplicate property that is assigned to another material does not affect the other material’s property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal