Editing material classes

  1. From the
    Material Classes
    dialog, select the class, and then click the
    Edit
    button. The
    Edit Material Class
    dialog opens.
    FTBMM_ED_odin_edit_material_class_general_1
  2. Make necessary changes, and then click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal