Creation binding
If you select
Class Based
, then you can select a class of units from
which a unit may be selected for binding. In the North_Parlor process cell there are two
units. Selecting MBR_FREEZER_CLS enables the FactoryTalk Batch Server or the operator to
choose from either NP_FREEZER1 or NP_FREEZER2.
Provide Feedback