Filter the asset list
Filter the asset list to quickly view the lifecycle status of an asset or assets. The filtered assets or devices' parent nodes are shown only in gray to keep the hierarchy relationship.
To filter the asset list
- SelectView > Assets Lifecycle, or click theAssets Lifecyclebutton.
- To filter assets on theAssettab, click theAssettab.To filter assets on theAsset Inventorytab, click theAsset Inventorytab.
- You can filter the asset by theBy Nameoption or theBy Statusoption.
- To filter assets by name, type the asset name in theBy Namebox.The assets including the name show immediately as you type.TIP:The name filter supports the wildcard "*" to filter the assets. For example, typingA*Cfilters assets whose names includeABC,ADC, and so forth.Clearing theBy Namebox shows all the assets.
- To filter assets by status, click theBy Statuslist and select a status.The assets of the selected status show in the list.TIP:SelectingAllin theBy Statuslist to show all the assets.
Provide Feedback