About the Content and Filters pane
The following tabs are shown only if a binder is selected in the asset tree or at the top of the
Archive
tab.- ContentShows a list of the files in the binder. In theHistoryorLabelstab, select the version of the binder for which you want to view the contents. If the binder contains folders and subfolders, use the tree on the left of theContenttab to navigate within the binder.
- FiltersFilters determine what files are included in the binder when the binder is checked in. In theHistoryorLabelstab, select the version of the binder for which you want to view the filters and then click theFilterstab.
Provide Feedback