Add Area
The user can add the Area under the Site. Perform the following steps to add an Area:
- On the left navigation menu, drop-down theConfigurationmenu and clickAsset Setup.
- Click theSitenode from the Hierarchy list.
- Click the [] icon and selectAdd Node.
- In theAdd Nodewindow, set these parameters:
- Select item type: Select the Area radio button in the left pane.
- Name: Provide the Area name.
- Description: Provide a description of the Area.
- Functional Location: Provide the location details.NOTE: Select theAuto Generate Functional Locationcheckbox to use the system-generated functional location.
- Configuration Status: By default, Configuration Status is in Draft, and the user can select the required status from the drop-down list.
- ClickAdd.Add Area Window"Area was added to hierarchy successfully" message is displayed.
- (Optional) In theInfotab, clickEditand perform the following actions:
- Geographical Location: Provide the Geographical Location details.
- Contact Details: Provide the Contact Details.
- Remarks: Provide the Remarks details.
- ClickSave.
Provide Feedback