Windows Authentication on OSI PI
To connect InfoPlatform with Historian, install the following:
- On the FT Historian server(s), runPI System Management Toolslocated underStart Menu>System Management Tools.System Management Tools
- OpenSecurity>Mapping & Trustsunder the ‘System Management Tools’.
- Click [Mapping] tab and click [Add New Mapping] icon as shown in the following image.Mappings & Trusts
- The ‘Add New Mapping’ dialog displays. Perform the following steps to add new PI Mapping.
- Click the ellipsis [
] icon to define the Windows Account.
Add New Mapping - The ‘Select User or Group’ dialog displays. Click [Advanced].Select User or Group
- Define the following properties and click [Find Now].
- Object Type
- Location
- Select a User from the list and click [OK].Select Windows Account
- Click [OK] and close the ‘Select User or Group’ dialog.Select User or Group
- Click ellipsis [
] icon.
- The ‘Select PI Identity, PI Group, or PI User’ dialog displays. Select the PI Users Type from the drop-down list and select theFTHEngineerto assign the new PI Identity. Click [OK].Select PI Identity
- Click [Create] to create the PI Mapping and close the Add New Mapping dialog.Create New Mapping
- The newly created PI Mapping displays in the Mappings list.Mapping List
Provide Feedback